Ensure continuity in the event of a short circuit on a terminal circuit

When defining the electrical architecture of medical locations, the hospital's various electrical protection must work in a coordinated manner, as required by the European installation standard HD 60364-7-710.

In the absence of selectivity, a terminal short circuit can trip upstream protection to turn off all or part of the medical facility.

Total selectivity ensures the activity and safety of patients can be maintained.

Selectivity
ENSURE COORDINATION
BETWEEN PROTECTION
Safety
ENSURE WITH
TAILOR-MADE PROTECTION

Understand the selectivity of electrical protection

The referenced media source is missing and needs to be re-embedded.

How to build the facility to always power the terminal circuits ?

The referenced media source is missing and needs to be re-embedded.

In order to continue supplying the other terminal circuits of the distribution panel of group 2 medical location, the short-circuit on a terminal circuit must not trip the upstream protection.

Socomec solution

MEDSYS  Isolated Power Supply

The MEDSYS  Isolated Power Supply, a complete IEC 61439-certified distribution panel for group 2 facilities, offers a wide range of terminal switchgear that meets selectivity requirements. Socomec also offers support for designer or installer to help with the choice, sizing and verification of the selectivity of the protections.