Safely add or hot-swap the power module of an UPS

To minimise the time wasted by external call-outs, the end user must be able to add or hot-swap the power module themselves.

To avoid any risk of compromising the protected application, the firmware must be fully compatible.

Any firmware incompatibility must be detected immediately, before the new module is integrated in parallel with the other power modules feeding the charge.

To avoid any risk of errors, the firmware's incompatibility must be resolved without humans having to intervene. To do this, it should be solved through an automatic alignment and self-configuration.

Adding or hot swapping a power module must be done with the load fully protected by the UPS in use.

Certainty
MAINTAIN IN LOAD
WHEN ADDING A MODULE
Upgrade
UPDATE FIRMWARE
WITHOUT HUMAN ERRORS

Replace your module in peace

Example of the steps to replacing a power module in use with automatic firmware alignment

The referenced media source is missing and needs to be re-embedded.

The firmware update operation is ensured without any interruption to the power.

On what basis to choose a firmware update?

The referenced media source is missing and needs to be re-embedded.

Choosing the firmware update process is critical to simplifying the process as much as possible, minimising any time-wasting and ensuring continuity of operation.

It is recommended to select an update process that does not require downloading, compatibility verification or specific tools. It must include an automatic procedure without human intervention and one that protects the application during the update.

Socomec solution

MODULYS UPS range

The MODULYS GP and MODULYS XL range of modular UPS incorporate all the easy and safe firmware update features.

This includes auto-alignment and self-configuration procedures without any special tools or human intervention.

The application load is protected throughout the process. This feature is exclusive to the MODULYS range and unique in the UPS industry.