Achieve full compliance easily and quickly

As Data Centres continue to power our digital economy, the EU Energy Efficiency Directive (EED), led by the European Parliament, introduces critical compliance requirements for facilities exceeding 500kW since its first adoption in 2012. This landmark legislation aims to reduce final energy consumption by 11.7% by 2030, requiring regular reporting of key energy metrics. With Data Centre electricity usage projected to surpass 1,000 TWh by 2026, these regulations are reshaping operational strategies across the industry. 
 

EED: what Data Centres need to know
 

Key milestones and targets

The Energy Efficiency Directive establishes a comprehensive framework for driving energy efficiency improvements across all sectors. First introduced in 2012, the directive has evolved significantly to meet increasingly ambitious climate goals: 

Year Milestone Target/Requirement
2012 Initial adoption First energy efficiency framework for buildings >1000m²
2018 First major revision Enhanced energy savings obligations
2023 Comprehensive update Focus on Data Centres with mandatory reporting
2024-2025 Increased annual savings Minimum 1.3% energy consumption reduction
2030 Binding EU-wide target 11.7% reduction in final energy consumption

How Article 7 drives annual savings for Data Centres

Article 7 establishes binding annual energy savings obligations for EU Member States, requiring them to achieve new savings each year from 2021 to 2030. For Data Centres, this translates into mandatory energy reduction targets and implementation of efficiency measures throughout operations.

How can Data Centres stay compliant?

Article 12 reporting scheme & European database

The requirements for all Data Centres over 500kW (article 12) impact both metering and monitoring. Data Centre operators must report key performance indicators to the European database by 15 September 2024, then by 15 May in 2025 and subsequent years. Mandatory reporting includes:

  • Energy consumption and power utilisation
  • Temperature set points
  • Waste heat utilisation
  • Water usage
  • Renewable energy share

 

PUE & Power Metering


Which metric measures the energy efficiency of Data Centres?

Power Usage Effectiveness (PUE) is the primary metric that measures Data Centre energy efficiency. Defined in EN 50600-4-2, PUE represents the ratio between total facility energy consumption and IT equipment energy usage. This critical indicator helps operators qualify their data centre's performance and identify opportunities for improvement.
 

Practical steps to install meters

To achieve compliance with the EED revisions quickly, introducing comprehensive metering to your Data Center infrastructure is essential. Our multi circuit Diris Digiware power monitoring system with solid, flexible or split core current sensors ideal for retrofit applications can be integrated throughout the entire power distribution network - from incoming supply to PDUs and busway tap-off units. This system delivers accurate measurement (class 0.5) at every level, crucial for calculating PUE and supporting Data Traffic Indicators in Energy Management Systems.

Drive efficiency with PUE

European Code of Conduct on Data Centre Energy Efficiency: best practices for >1 MW sites

Modular UPS selection for medium-sized enterprises

Ian Tanti explains:

 

"If we consider section 6 of the EU code of conduct – 2024 best practice guidelines, we see the call for modular and scalable UPS systems, smart conversion operating modes and efficient part load operation – Energy Saver."

 

The EED mandates "elite" efficiency UPS systems with:

  • 93.5% efficiency in VFI mode
  • 98% efficiency in VFD mode
  • Class 1 compliance with IEC 60240-3 standard

Socomec's Modulys and Delphys UPS ranges deliver elite-level efficiency in compliance with the EU Code of Conduct, featuring plug-and-play power modules for seamless capacity expansion.
 

Learn about modular UPS
 

Rightsizing to cut operational efficiency gaps

"By rightsizing correctly, you limit your CapEx and optimise energy efficiency – and you also minimise energy losses," notes Ian. This approach allows facilities to grow as needed rather than deploying total capacity upfront. The Modulys XM has been engineered to outlive the applications it powers, eliminating costly replacements while supporting the EUDCA's sustainability goals. Rightsizing through modularity reduces wasted capacity between projected and actual future loads, while rapid repair capabilities significantly reduce MTTR despite maintaining attractive MTBF values.
 

Scalable energy management systems

"The foundations of compliance are built on permanent measuring solutions, not relying on temporary measurement campaigns that use portable equipment," explains Ian Tanti. "Today's energy management systems evolve with your electrical distribution, making it simple to scale without disruption."

“Versatility is so important. You must allow for rich measurements at any point - incoming, individual outgoing, AC and DC circuits. Above all, the measurements must be accurate - what that means is that they must be reliable and repeatable - even under really low load levels.”

FAQ: Energy Efficiency Directive PDF, reporting and more

Where can I download the EED PDF?

The official Energy Efficiency Directive PDF is available for download from the EU Publications Office website. The recast directive (EU) 2023/1791 was published in the EU Official Journal in September 2023.
 

What is the deadline for first-time reporting?

The first-time reporting deadline was rescheduled to 15 September 2024, with subsequent annual reporting due by 15 May 2025 and every year thereafter for data centres with IT power demand of at least 500kW.
 

Does the Directive apply to data centre computer rooms under 500 kW?

No, the EED reporting requirements specifically target data centre computer rooms with an IT power demand of at least 500kW. Smaller facilities are currently exempt from these mandatory reporting obligations.
 

How does the EED affect the footprint of data centres?

The EED drives reduced footprint of data centres by mandating energy efficiency improvements, promoting renewable energy integration, and requiring waste heat utilisation reporting to support the EU's 11.7% energy reduction target by 2030.
 

What role does an energy management system play?

An energy management system is essential for monitoring consumption, optimising power usage, and ensuring compliance with EED requirements. It provides the accurate data needed for mandatory reporting and identifies efficiency improvement opportunities.µ
 

What are the EU energy efficiency targets for 2030?

By 2030, Member States must achieve at least 11.7% reduction in final energy consumption compared to projected use, with an overall goal of cutting primary energy consumption by 39%. These targets are legally binding and apply across all sectors, including Data Centers. For operators, this means implementing continuous monitoring, adopting best-practice efficiency measures, and documenting energy savings to demonstrate compliance with the directive. 
 

What is the article 12 of the EU EED?

Article 12 of the EU EED sets out rules to remove barriers to energy efficiency in energy supply and consumption. It requires Member States to promote efficient heating and cooling, improve transformation, transmission and distribution systems, and enable demand response through smart energy management.

Ian Tanti
Ian Tanti
Segment & Specification Manager Socomec Group

" Operators will need to move swiftly to understand the implications of these new rules - and to ensure compliance.  Interpreting the revisions to EED targets and their impact on Data Centres requires a degree of analysis in order to make sure that facilities are not only optimising efficiencies for sustainability, cost-effectiveness and environmental stewardship, but that they’re fully aligned with the new legislation. ”

Contact us